AXIS#.VL.ARTYPE1 to AXIS#.VL.ARTYPE4

Description

These parameters indicate the method used to calculate the biquad coefficients AXIS#.VL.ARPFx, AXIS#.VL.ARPQx, AXIS#.VL.ARZFx, and AXIS#.VL.ARZQx. A value of 0 indicates that the coefficients are set directly. This parameter has no effect on the filter itself, but is only used to determine the original design parameters.

Value Definition
0 Unity: Biquad is in a pass-through state, unity at all frequencies
1 Lowpass: Standard two-pole lowpass filter
2

Notch/Resonator: A standard Notch filter with selectable bandwidth, frequency and depth - can also be used to create a positive notch(Resonator) by making the gain positive

3

Lead/Lag: Filter with unity gain at low frequencies and either high gain (Lead) or low gain (Lag) at high frequencies, with the center frequency and gain user selectable

4

Biquad: Biquad is opened up with raw values on the numerator and denominator for the user to customize.

5

Auto-tuned Biquad: This means the filter was tuned by the Autotuner - manually changing this filter cannot guarantee stability.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 5

Default Value

AXIS#.VLARTYPE1 = 1

AXIS#.VLARTYPE2 = 4
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
AXIS1.VL.ARTYPE1

5011h

0ch

Signed8

-

-

Read/Write

No

AXIS1.VL.ARTYPE2

5011h

0dh

Signed8

-

-

Read/Write

No

AXIS1.VL.ARTYPE3

5011h

0eh

Signed8

-

-

Read/Write

No

AXIS1.VL.ARTYPE4

5011h

0fh

Signed8

-

-

Read/Write

No

AXIS2.VL.ARTYPE1

5111h

0ch

Signed8

-

-

Read/Write

No

AXIS2.VL.ARTYPE2

5111h

0dh

Signed8

-

-

Read/Write

No

AXIS2.VL.ARTYPE3

5111h

0eh

Signed8

-

-

Read/Write

No

AXIS2.VL.ARTYPE4

5111h

0fh

Signed8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.ARTYPE1

6008

1778

Signed8

Read/Write

-

AXIS2.VL.ARTYPE1

71544

1177

Signed8

Read/Write

-

AXIS1.VL.ARTYPE2

6009

1779

Signed8

Read/Write

-

AXIS2.VL.ARTYPE2

71545

1177

Signed8

Read/Write

-

AXIS1.VL.ARTYPE3

6010

177A

Signed8

Read/Write

-

AXIS2.VL.ARTYPE3

71546

1177

Signed8

Read/Write

-

AXIS1.VL.ARTYPE4

6011

177B

Signed8

Read/Write

-

AXIS2.VL.ARTYPE4

71547

1177

Signed8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.ARTYPE1

6008

Signed8

Read/Write

-

AXIS#.VL.ARTYPE2

6009

Signed8

Read/Write

-

AXIS#.VL.ARTYPE3

6010

Signed8

Read/Write

-

AXIS#.VL.ARTYPE4

6011

Signed8

Read/Write

-